C optimization for calculating a real norm square of 16bits vector

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C optimization for calculating a real norm square of 16bits vector

Jump to solution
2,759 Views
shoham
Contributor I

Hello,

I'm working with CodeWarrior  Version: 10.1.8 Build Id:158.

I've tried to write an optimize function to calculate:    output  = A' x A   <==> output = Dot Product(A , A) 

 

Word40 DOT_XX_40Bits(Word16 * restrict a_pV1, int N)

{

#pragma opt_level = "O3"

      int i;

      Word40 Results, Sum1 = X_extend(0), Sum2= X_extend(0);

      int* pV32_1 = (int*)a_pV1;

      int __SR__ = readSR();  setnosat();

      cw_assert((int)a_pV1%8==0); cw_assert(N>=64);cw_assert( N%8 == 0 );

 

      for(i=0; i<N/2; i+=2)  

{

            Sum1 = X_macd(Sum1, pV32_1[i+0], pV32_1[i+0]);

            Sum2 = X_macd(Sum2, pV32_1[i+1], pV32_1[i+1]);

      }

 

      Sum1        = X_add (Sum1, Sum2);

      Results     = X_asr (Sum1);

      writeSR(__SR__);

      return Results;

}

 

The inner Assembly loop is as follows:

  

    LOOPSTART3                  

[

    macd     d2,d2,d4                   

    macd     d3,d3,d6                  

    move.2l  (r0)+,d2:d3           

 ]

    LOOPEND3

 

50% efficiency!

 

I've tried to unroll the C loop (more):

      for(i=0; i<N/2; i+=4)  

{

            Sum1 = X_macd(Sum1, pV32_1[i+0], pV32_1[i+0]);

            Sum2 = X_macd(Sum2, pV32_1[i+1], pV32_1[i+1]);

            Sum3 = X_macd(Sum3, pV32_1[i+3], pV32_1[i+3]);

            Sum4 = X_macd(Sum4, pV32_1[i+4], pV32_1[i+4]);

}

But the result was worse (lack of register in inner loop!?).

 

 - Note that the unrool pragma doesn't work (and I'll be glad to understand way?).

 

Please help me understand how should I do it right (100% efficiency in inner loop)?

 

Thanks,

Perry Shoham




Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,161 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Perry,

 

I think you have run into a so called "mixed optimization level" case.

In your project, in think, from command line (Project Settings) you have set the optimization level to O0 and from file, via pragma, you have set O3.

 

In this case the registers allocation is done by the high-level optimizer (-O0 command line option) and not by the low-level optimizer (valid only in -03 command line).

 

In order to fix this problem, please go to project properties or file properties (in case you want to specify only for the file that contains the function) and change the optimization level to O3.

In the same time you can comment the //#pragma opt_level = "O3" from the function body.

 

In this way you will obtain:

 

LOOPSTART3

DW10 TYPE debugsymbol

[

macd d0,d0,d9 ;[43,1] 1%=1 [0]

macd d1,d1,d4 ;[44,1] 1%=1 [0]

macd d2,d2,d5 ;[46,1] 1%=1 [0]

macd d3,d3,d8 ;[0,1] 1%=1 [0]

move.2l (r0)+n3,d0:d1 ;[43,1] 0%=0 [1]

move.2l (r1)+n3,d2:d3 ;[46,1] 0%=0 [1]

]

LOOPEND3

 

Hope this will help you.

 

Best regards,

 

View solution in original post

0 Kudos
Reply
4 Replies
2,161 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello,

 

Have you tried to rewrite the loop in order to use 2 restrict pointers (pV32_1 and pV32_2) in order to compute Sum1 and Sum2?

In this case the compiler should generate 2 moves in parallel in the inner loop.

 

Best regards.

0 Kudos
Reply
2,161 Views
shoham
Contributor I

Hi,

Here the result:

 

    LOOPSTART3                  

 [

    macd     d10,d10,d6                 ;[114,1] 2%=1 [0]

    macd     d11,d11,d8                 ;[0,1] 2%=1 [0]

    move.2l  (r0)+n3,d10:d11            ;[112,1] 0%=0 [1]

 ]

 [

    macd     d10,d10,d2                 ;[112,1] 1%=0 [1]

    macd     d11,d11,d4                 ;[113,1] 1%=0 [1]

    move.2l  (r1)+n3,d10:d11            ;[114,1] 1%=0 [1]

 ]

    LOOPEND3   

 

Here is the source code:

#define DOT_XX_40Bits_UNROOL_LOOP 4Word40 DOT_XX_40Bits(Word16 * restrict a_pV1, Word16 * restrict a_pV2, int N){#pragma opt_level = "O3"#pragma noinline int i; Word40 Results, Sum1, Sum2, Sum3, Sum4; int* pV32_1 = (int*)a_pV1; int* pV32_2 = (int*)a_pV2;  int __SR__ = readSR(); setnosat();  Sum1 = X_extend(0); Sum2 = X_extend(0); Sum3 = X_extend(0); Sum4 = X_extend(0);     cw_assert((int)a_pV1%8==0);    cw_assert((int)a_pV2%8==0);    cw_assert((int)pV32_1%8==0);    cw_assert((int)pV32_2%8==0);    cw_assert(N>=64);    cw_assert( N%8 == 0 ); for(i=0; i<N/2; i += DOT_XX_40Bits_UNROOL_LOOP) {  Sum1 = X_macd(Sum1, pV32_1[i+0], pV32_1[i+0]);  Sum2 = X_macd(Sum2, pV32_1[i+1], pV32_1[i+1]);#if(DOT_XX_40Bits_UNROOL_LOOP==4)    Sum3 = X_macd(Sum3, pV32_2[i+2], pV32_2[i+2]);  Sum4 = X_macd(Sum4, pV32_2[i+3], pV32_2[i+3]);#endif }#if(DOT_XX_40Bits_UNROOL_LOOP==2) Sum1   = X_add (Sum1, Sum2); Results  = X_asr (Sum1);#elif(DOT_XX_40Bits_UNROOL_LOOP==4) Sum1   = X_add (Sum1, Sum2); Sum3   = X_add (Sum3, Sum4); Sum1   = X_asr (Sum1); Sum3   = X_asr (Sum3); Results  = X_add (Sum1, Sum3);#endif    writeSR(__SR__); if( (_readEMR() & (1<<2)) ) stop(); return Results;}

          

Best regards,

Perry        

0 Kudos
Reply
2,162 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Perry,

 

I think you have run into a so called "mixed optimization level" case.

In your project, in think, from command line (Project Settings) you have set the optimization level to O0 and from file, via pragma, you have set O3.

 

In this case the registers allocation is done by the high-level optimizer (-O0 command line option) and not by the low-level optimizer (valid only in -03 command line).

 

In order to fix this problem, please go to project properties or file properties (in case you want to specify only for the file that contains the function) and change the optimization level to O3.

In the same time you can comment the //#pragma opt_level = "O3" from the function body.

 

In this way you will obtain:

 

LOOPSTART3

DW10 TYPE debugsymbol

[

macd d0,d0,d9 ;[43,1] 1%=1 [0]

macd d1,d1,d4 ;[44,1] 1%=1 [0]

macd d2,d2,d5 ;[46,1] 1%=1 [0]

macd d3,d3,d8 ;[0,1] 1%=1 [0]

move.2l (r0)+n3,d0:d1 ;[43,1] 0%=0 [1]

move.2l (r1)+n3,d2:d3 ;[46,1] 0%=0 [1]

]

LOOPEND3

 

Hope this will help you.

 

Best regards,

 

0 Kudos
Reply
2,161 Views
shoham
Contributor I

Hi,

You are absolutely right,

I've changed the optimization file,  removed the extra input a_pV2 and left the "manual" unroll x 4 loop.

And got the 100% optimization.

Thanks a lot & regards,

Perry

0 Kudos
Reply