Memory browser vs mem command with Debugger Shell

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory browser vs mem command with Debugger Shell

Jump to solution
2,646 Views
klm78
Contributor I

Hi,

We have some doubt concerning the memory browser window in CW 10.1.8 for StarCore.

Our Configuration is ADS8156

If we open this browser at a memory adress in DDR > 0x40000000 and look at the same adress  with Debugger Shell mem command

The result is the same.

If we modify  a value memory cell in the browser, there's no change observed with mem command in Debugger Shell

 

 

Which way is the most accurate for dumping memory in Debug Mode ?

 

Is this issue could be due to CACHE management ?

 

Thanks in advance

 

BR. klm78

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,260 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi klm78,

 

Seems to be indeed a cache related behavior. I'll check this and return with details as soon as I'll have access to a board.

 

Nonetheless, the preferred way of dumping memory are Target Tasks/Import-Export memory.

Also, please be aware that there are two types of Memory views supported in CW - one of them is the Memory Browser view with a reduce set of features and the other one is Memory view. 

 

I advice you to use the Memory view, where you can place a monitor (for example at 0x40000000) and in the same time you can specify which type of memory is used (physical, virtual for data or virtual for program)

 

Hope this helps.

View solution in original post

0 Kudos
Reply
1 Reply
2,260 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi klm78,

 

Seems to be indeed a cache related behavior. I'll check this and return with details as soon as I'll have access to a board.

 

Nonetheless, the preferred way of dumping memory are Target Tasks/Import-Export memory.

Also, please be aware that there are two types of Memory views supported in CW - one of them is the Memory Browser view with a reduce set of features and the other one is Memory view. 

 

I advice you to use the Memory view, where you can place a monitor (for example at 0x40000000) and in the same time you can specify which type of memory is used (physical, virtual for data or virtual for program)

 

Hope this helps.

0 Kudos
Reply