Build at Optimization level O3 fails - Release configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build at Optimization level O3 fails - Release configuration

ソリューションへジャンプ
2,246件の閲覧回数
ITCO00
Contributor III

Hi,

 

I'm working with CW toolset 10.1.3 for SmartDSP MSC8156.

I've a 'C' compiled successfully at optimization O0, but at optimization level O3 it fails. 

Preprocessing - produces the same text.

file size - ~17kb

Attached - verbose output  of the compilation process; 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,553件の閲覧回数
CrasyCat
Specialist III

I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach the preprocessing listing file and indicate which compiler options you are using for building.

 

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,554件の閲覧回数
CrasyCat
Specialist III

I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach the preprocessing listing file and indicate which compiler options you are using for building.

 

 

CrasyCat

0 件の賞賛
返信