Build Error - LLT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Error - LLT

Jump to solution
2,632 Views
ITCO00
Contributor III

Hello,

 

I'm using CW 10.1.3 for MC8156 SmartDSP.

While building a specific C file (size is ~45Kb) in optimization level 3, I've received the following error:

RA ERROR 2: Temporary spill variable spilled. PROCESS IS TERMINATED

What does it mean?

 

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,111 Views
CrasyCat
Specialist III

Hello

 

Can you give it a try with CodeWarrior for Starcore V10.1.5, which is available from our download page

(http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-STARCORE-DSP10&fpsp=1&tab=Design_T...

 

There were a couple of these "RA ERROR 2: Temporary spill variable spilled" errors fixed in there.

If the issue is still present, please submit a service request at following URL:

    https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR

 

make sure to attach the preprocessor listing for the source file generating the issue as well as the command line options you are using to build.

 

 

CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
2,112 Views
CrasyCat
Specialist III

Hello

 

Can you give it a try with CodeWarrior for Starcore V10.1.5, which is available from our download page

(http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-STARCORE-DSP10&fpsp=1&tab=Design_T...

 

There were a couple of these "RA ERROR 2: Temporary spill variable spilled" errors fixed in there.

If the issue is still present, please submit a service request at following URL:

    https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR

 

make sure to attach the preprocessor listing for the source file generating the issue as well as the command line options you are using to build.

 

 

CrasyCat

0 Kudos
Reply