uboot_ddr1.c to U-Boot 2021.04 integration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot_ddr1.c to U-Boot 2021.04 integration

1,333件の閲覧回数
rudolfusselmann
Contributor II

Hello,

We have configured our DDR4 with QCVS and generated the code for U-Boot.

However, we only could find AN5279 that explains the integration for an older U-Boot for LS2080. We are using LS1046A.

Are there any guides, as to how to integrate the DDR configuration with U-Boot 2021.4 ?

Has anyone done this and can offer some guidance?

Many Thanks,

rudi

タグ(3)
0 件の賞賛
返信
1 返信

1,307件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In the recent released LSDK, we use ATF rather than using u-boot directly, DDR initialization is performed in ATF not in u-boot.

You could download LSDKUG_Rev21.08.pdf and refer to section "5.2.1.1 TF-A DDR Driver".

If you only use u-boot, you could still refer to AN5279.

0 件の賞賛
返信