uart0 console;messy code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uart0 console;messy code

1,743 次查看
连营张
Contributor I

hello,i'm working on the p2041rdb.i reflashed the p2041rdb NOR flash image(QorIQ_SDK_V1.4_P2041RDB_20130625_NOR_Flash.bin),after that i found the uart0 console don't print boot message,only showing messy code.that's why?please help me.the serial baud rate is 115200,none flow control.

标签 (1)
0 项奖励
回复
2 回复数

1,594 次查看
连营张
Contributor I

i guess that the uart0 is corrupted.can i redirect the boot messages to uart1?

0 项奖励
回复

1,594 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please create a CodeWarrior bareboard sample project, and execute this project, as normal you will see "Hello CodeWarrior!" from UART0 after executing this program. This could help you to make decision whether it is the problem of image or UART0 on the target board.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复