uart0 console;messy code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uart0 console;messy code

1,747件の閲覧回数
连营张
Contributor I

hello,i'm working on the p2041rdb.i reflashed the p2041rdb NOR flash image(QorIQ_SDK_V1.4_P2041RDB_20130625_NOR_Flash.bin),after that i found the uart0 console don't print boot message,only showing messy code.that's why?please help me.the serial baud rate is 115200,none flow control.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,598件の閲覧回数
连营张
Contributor I

i guess that the uart0 is corrupted.can i redirect the boot messages to uart1?

0 件の賞賛
返信

1,598件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please create a CodeWarrior bareboard sample project, and execute this project, as normal you will see "Hello CodeWarrior!" from UART0 after executing this program. This could help you to make decision whether it is the problem of image or UART0 on the target board.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信