seeking MCF52235 UDP application, simple TCP/IP STACK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

seeking MCF52235 UDP application, simple TCP/IP STACK

3,745 Views
internike
Contributor I
Interniche stack provided by Freescale on ColdFire EVB is quite complicated!
Does anyone have modified it for a simple UDP protocol application?
 
Regards, Luigi
 
Labels (1)
0 Kudos
Reply
3 Replies

1,134 Views
internike
Contributor I
Hi Mark, thanks for your attention about my necessities!
 
I'like to know how to get the CW 6.3 project, in order to test it.
 
Thanks, Luigi
0 Kudos
Reply

1,134 Views
mjbcswitzerland
Specialist V
Hi Luigi

Please go to http://www.utasker.com/Licensing/License.html to see the licensing terms. Then return the simple application form on that page or here: http://www.utasker.com/Licensing/License.txt

Important: Please note that we use the application information to help define the best package for your requirement and also as a reference when giving support. No information is made available to third parties or used for advertising etc.

After application (for educational/hobby, evaluation or commercial use as appropriate) you will receive the complete project including source and a powerful simulator. This is set up for CW6.3 on the EVB or DEMO board.

If you would like to simply run the uTasker demo project on your hardware you can freely try this by downloading the target code from the software page:
http://www.utasker.com/software/software.html

The default IP address of the board will be 192.168.0.3 and can then be changed and saved via web browser, Telnet or UART. Follow the step-by-step instructions for loading to your board in the Coldfire tutorial:
http://www.utasker.com/docs/M5223X/uTaskerV1.2-Tutorial-M5223X.PDF

The default web pages are also at the software link. You can change them if you wish and simply load them via FTP to the target.

I look forward to hearing from you again.

Regards

Mark
0 Kudos
Reply

1,134 Views
mjbcswitzerland
Specialist V
Hi Luigi

Try the uTasker stack (www.uTasker.com). It is free for non-commercial work and fully supported - even for students.
It was designed especially for educational purposes (as well as serious commercial projects) and so is easy to understand and fun to work with.
It is delivered with a fully functional M5223X project for CW6.3 including tutorial and a real-time simulator allowing the project also to be tested and further developed on a PC.

There are online demos:
http://212.254.22.36
http://212.254.22.36:8080 (web cam to see demo)
http://212.254.22.36:8081/0 (LCD controlled via Browser - see also on web cam)

As well as the TCP/IP stack it is a RTOS and has most device drivers (3 x UART in interrupt or DMA modes, QSPI, ADC, CAN, I2C, Ethernet, FLASH File system) and also supports an external file system via SPI EEPROM.

Regards

Mark Butcher
www.mjbc.ch / www.uTasker.com
0 Kudos
Reply