ethernet tap netparam

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ethernet tap netparam

跳至解决方案
1,546 次查看
iv
Contributor I

Hi,

i'm working on CW with ethernet tap rev b on target p3041.

I did a wrong command with netparam on telnet shell ("netparam bootconfig static") without ip and now the tap is unreachable.
Is it possible to rectify this parameter?

thks
标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,412 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

You should connect your broken etap to your computer using an usb wire. It's not very difficult to fix back the networks params - just let the etap boots up and use a serial terminal to write the inputs (the help command is all you need).

Regards,

Marius

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,412 次查看
iv
Contributor I

ok thanks,i used screen on /dev/ttyACM0.

0 项奖励
回复
1,413 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

You should connect your broken etap to your computer using an usb wire. It's not very difficult to fix back the networks params - just let the etap boots up and use a serial terminal to write the inputs (the help command is all you need).

Regards,

Marius

0 项奖励
回复