Where is apptrk for P1020WLAN?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is apptrk for P1020WLAN?

Jump to solution
1,505 Views
larryharmon
Contributor II

I am using a P1020WLAN development system.

I have downloaded and installed (with much difficulty) CodeWarrior development Studio for Power Architecture Processors Linux Edition v8.8.

 

After installition the documentation says to run apptrk :1000 on the target system.

This application is not found on my new P1020WLAN.


Labels (1)
0 Kudos
Reply
1 Solution
1,321 Views
larryharmon
Contributor II

So, if I understand correctly, I need to build a new file system with apptrk included, then reflash the P1020WLAN with the new file system.  Or possible put the new FS on a USB stick and use it from there?

View solution in original post

0 Kudos
Reply
4 Replies
1,321 Views
marius_grigoras
NXP Employee
NXP Employee

P1020WLAN is not supported in CW8.8.

But..regarding the apptrk support it should work because the e500v2 core is supported in CW classic. The apptrk support is not board specific.

Regards,

Marius

0 Kudos
Reply
1,321 Views
larryharmon
Contributor II

But apptrk doesn't seem to be installed!  How do I get it on the P1020WLAN?

0 Kudos
Reply
1,321 Views
marius_grigoras
NXP Employee
NXP Employee

It comes with the Linux SDK.

Marius

1,322 Views
larryharmon
Contributor II

So, if I understand correctly, I need to build a new file system with apptrk included, then reflash the P1020WLAN with the new file system.  Or possible put the new FS on a USB stick and use it from there?

0 Kudos
Reply