ethernet tap netparam

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ethernet tap netparam

ソリューションへジャンプ
2,244件の閲覧回数
iv
Contributor I

Hi,

i'm working on CW with ethernet tap rev b on target p3041.

I did a wrong command with netparam on telnet shell ("netparam bootconfig static") without ip and now the tap is unreachable.
Is it possible to rectify this parameter?

thks
ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,110件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

You should connect your broken etap to your computer using an usb wire. It's not very difficult to fix back the networks params - just let the etap boots up and use a serial terminal to write the inputs (the help command is all you need).

Regards,

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,110件の閲覧回数
iv
Contributor I

ok thanks,i used screen on /dev/ttyACM0.

0 件の賞賛
返信
2,111件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

You should connect your broken etap to your computer using an usb wire. It's not very difficult to fix back the networks params - just let the etap boots up and use a serial terminal to write the inputs (the help command is all you need).

Regards,

Marius

0 件の賞賛
返信