error:Stepping using step range is taking too long,resuming process.  what is problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error:Stepping using step range is taking too long,resuming process.  what is problem

2,894件の閲覧回数
sunwind45
Contributor I
CodeWarrior for PPC:smileyfrustrated:tepping using step range is taking too long,resuming process.
 
give me a idea about it!
 
thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,677件の閲覧回数
Black
Contributor I

If you step over a function and the target doesn't stop (the CodeWarrior Debugger cannot read the PC) then this error is returned. A CodeWarrior CCS log could help tracking down this issue (in Project Settings, Remote Debugging panel, select Edit Connection and check Enable Logging).

I hope this helps.

0 件の賞賛
返信

1,677件の閲覧回数
sunwind45
Contributor I
Thanks for your idea.
I'll  try it. 
 
Otherwise,
This error is returned when loading the object file into mpc862 using PowerTAP Emulator.
 
Is the hardware bad? Or mpc862 is bad? Or BDM on mpc862 is bad?
0 件の賞賛
返信