convert pascal code for 68k mac to pc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

convert pascal code for 68k mac to pc

1,808件の閲覧回数
Leroy
Contributor I
Hi:
is there a short version method to convert 68k mac pascal to something that will run on a pc? 1700 lines

thanks
Leroy
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,010件の閲覧回数
mke_et
Contributor IV
Well, first I'd get a compatible pascal compiler. And no matter what you get, there's sure to be 'issues'.

If it's a 'processing' program, you're still going to have to contend with how data gets in and goes out of the program, that may bring up different issues on a PC than on a Mac.

If you mean a GUI program watch out. Delpi had a program to let PC stuff run on a unix type platform, but I would suspect that a lot of it is an interface layer that assumes you start on the PC and then does some kind of translation to a unix interface layer. Sorry, but I don't really know. I've got the package in a drawer somewhere but never used or even installed it.

I would say your best bet is to contact the language vendor for the package you're now using and see what they offer. Then decide.

If it's REALLY bad, and you have to manually do it, I'd set up a PC and a Mac next to each other, start by copying the screens, and then doing it event by event for the screen items. Won't be simple.
0 件の賞賛
返信