convert pascal code for 68k mac to pc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

convert pascal code for 68k mac to pc

1,849 Views
Leroy
Contributor I
Hi:
is there a short version method to convert 68k mac pascal to something that will run on a pc? 1700 lines

thanks
Leroy
Labels (1)
0 Kudos
Reply
1 Reply

1,051 Views
mke_et
Contributor IV
Well, first I'd get a compatible pascal compiler. And no matter what you get, there's sure to be 'issues'.

If it's a 'processing' program, you're still going to have to contend with how data gets in and goes out of the program, that may bring up different issues on a PC than on a Mac.

If you mean a GUI program watch out. Delpi had a program to let PC stuff run on a unix type platform, but I would suspect that a lot of it is an interface layer that assumes you start on the PC and then does some kind of translation to a unix interface layer. Sorry, but I don't really know. I've got the package in a drawer somewhere but never used or even installed it.

I would say your best bet is to contact the language vendor for the package you're now using and see what they offer. Then decide.

If it's REALLY bad, and you have to manually do it, I'd set up a PC and a Mac next to each other, start by copying the screens, and then doing it event by event for the screen items. Won't be simple.
0 Kudos
Reply