convert pascal code for 68k mac to pc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

convert pascal code for 68k mac to pc

1,839 次查看
Leroy
Contributor I
Hi:
is there a short version method to convert 68k mac pascal to something that will run on a pc? 1700 lines

thanks
Leroy
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,041 次查看
mke_et
Contributor IV
Well, first I'd get a compatible pascal compiler. And no matter what you get, there's sure to be 'issues'.

If it's a 'processing' program, you're still going to have to contend with how data gets in and goes out of the program, that may bring up different issues on a PC than on a Mac.

If you mean a GUI program watch out. Delpi had a program to let PC stuff run on a unix type platform, but I would suspect that a lot of it is an interface layer that assumes you start on the PC and then does some kind of translation to a unix interface layer. Sorry, but I don't really know. I've got the package in a drawer somewhere but never used or even installed it.

I would say your best bet is to contact the language vendor for the package you're now using and see what they offer. Then decide.

If it's REALLY bad, and you have to manually do it, I'd set up a PC and a Mac next to each other, start by copying the screens, and then doing it event by event for the screen items. Won't be simple.
0 项奖励
回复