codewarrior usb tap firmware update problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior usb tap firmware update problem

2,402 Views
wangcuixmwangcu
Contributor III

I got a codewarrior usb tap, its version is 900-75115 REV C.

I want update its firmware through codewarrior IDE 10.4.

Can it supoort more devices?

0 Kudos
Reply
1 Reply

2,115 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello wangcuixm wangcuixm,

For USB TAP Firmware updating, please use the following procedure.
Please open CCS from Start->Programs->Freescale CodeWarrior->CW for PA <version>->CodeWarrior Connection Server, and type the following commands.
(bin) 93 % config cc utap
(bin) 94 % show cc
0: USB TAP (JTAG) (utap:) Loader software ver. {1.0} Sending code to USB TAP - please wait
0: USB TAP (JTAG) (utap:) CC software ver. {1.3}

To update the flash…

(bin) 96 % delete all
(bin) 97 % updateutap
USB TAP Loader current software ver. {1.0} Sending code to USB TAP - please wait

*** WARNING ***

DO NOT UNPLUG YOUR USB TAP: Doing so will render your USB TAP non-functional and require factory reprogramming.
Please wait until the alternating Yellow/Green RUN/PAUSE light turns off.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply