.bss into NVM i.e. treated as .data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.bss into NVM i.e. treated as .data

Jump to solution
2,028 Views
CarlFST60L
Senior Contributor II

 Hi,

 

I have posted in another section of the forums, though I am not sure it is the correct area:

 

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=8024

 

We are using MRAM on the 52259evb and really need to work out how we get .bss to be treated the same as .data for the S19 so it programs the value in MRAM when set as 0.

 

Logically I can see various solutions, however, its making the application development far more complicated (due to backward / forward compatibiliy for remote firmware updating, data initilizing etc).

 

If we could just force varbiles to be created as .data instead of .bss all our problems would be solved.

 

PS Codewarrior 7.1.2 build 11

Message Edited by CarlFST60L on 2009-10-26 12:58 AM
Labels (1)
0 Kudos
Reply
1 Solution
1,332 Views
CrasyCat
Specialist III
0 Kudos
Reply
1 Reply
1,333 Views
CrasyCat
Specialist III

Hello

 

This one has been answered under

 

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=8024

 

 

CrasyCat

0 Kudos
Reply