.bss into NVM i.e. treated as .data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

.bss into NVM i.e. treated as .data

ソリューションへジャンプ
2,037件の閲覧回数
CarlFST60L
Senior Contributor II

 Hi,

 

I have posted in another section of the forums, though I am not sure it is the correct area:

 

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=8024

 

We are using MRAM on the 52259evb and really need to work out how we get .bss to be treated the same as .data for the S19 so it programs the value in MRAM when set as 0.

 

Logically I can see various solutions, however, its making the application development far more complicated (due to backward / forward compatibiliy for remote firmware updating, data initilizing etc).

 

If we could just force varbiles to be created as .data instead of .bss all our problems would be solved.

 

PS Codewarrior 7.1.2 build 11

Message Edited by CarlFST60L on 2009-10-26 12:58 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,341件の閲覧回数
CrasyCat
Specialist III
0 件の賞賛
返信
1 返信
1,342件の閲覧回数
CrasyCat
Specialist III

Hello

 

This one has been answered under

 

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=8024

 

 

CrasyCat

0 件の賞賛
返信