Using CodeWarrior QCVS Generate_Code in U-Boot for p2041 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using CodeWarrior QCVS Generate_Code in U-Boot for p2041 custom board

2,029 Views
ilyakrasavin
Contributor I

Hi.

I am working with the custom p2041 board based on p2041RDB. The am is different from RDB and there is no I2C EPROM for parameters. I have QCVS generated code for my RAM.

How to modify yocto based u-boot (NXP SDK) to adopt this difference? (what files I need to change ?)

Since I've not used to work with yocto - please give me commands sequence that will produce the tree, that I can use and modify later.

Thanks,

Ilya

Tags (2)
0 Kudos
Reply
1 Reply

1,752 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ilya Krasavin,

I explain something about how to use DDRv tool.

If there is SPD on the target board, the user can use reading from SPD method to create and initial QCVS DDR project. If there is no SPD, the user needs to create a default QCVS project, then fill DDR related properties according to DDR data sheet to generate the initial DDR controller configuration parameters.

Then use DDRv tool to connect to the target board to do optimization and validation, the user needs to complete "Centering the clock", "Read ODT and driver" and "Write ODT and dirver" validations to get the final optimized DDR controller configuration parameters.

You could refer to the document "QCVS DDR Tool User Guide" from NXP Semiconductors | Automotive, Security, IoT.

After validation with DDRv in QCVS project, please regenerate DDR configuration script from Project->Generate Processor Expert code, then use DDR controller configuration parameters in script ddrCtrl_1.py in u-boot or DDR initialization file.

If there is SPD on your target, please modify the structure  "board_specific_parameters dimm0" in board/freescale/p2041rdb/ddr.c according to the optimized DDR related parameters.

You could refer to this document DDR Controller Configuration on LS2085/LS2080 Bringing up.

If there is no SPD on the target board, you could use raw timing or fixed DDR configuration parameter.

For Raw Timing configuration method, please refer board/freescale/p1023rdb/ddr.c.

For fixed DDR parameters configuration, please refer to board/freescale/corenet_ds/p4080ds_ddr.c


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply