Target processor setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Target processor setting

ソリューションへジャンプ
2,607件の閲覧回数
Chanh
Contributor III

Hi,

I am using CodeWarrior for QorIQ LS Series with FRWY-LS1046A board, I follow the user manual to create bare metal project. When I go the the setting page, the target processor is cortex-m3 and cannot be changed. May I know any problem with that option if I run the binary file on the board? And how to change the processor to cortex-a72?

Thanks.

0 件の賞賛
返信
1 解決策
2,602件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

No need to do modification, please use the default setting, this option will not be used in the compilation.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,591件の閲覧回数
Chanh
Contributor III

Hi Yiping,

Got it. Thanks.

0 件の賞賛
返信
2,603件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

No need to do modification, please use the default setting, this option will not be used in the compilation.

0 件の賞賛
返信