SerDes configuration issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SerDes configuration issue

1,564 Views
tungnguyen
Contributor I

Dear Sir/Madam,

 

I have the problem on QorIQ for T2080 "serdes configuration when probe targget when using codewarrior tap". I try 3 cases:

 

Case 1: using Nand boot, run DDRv Tool. Results: probe target is ok, i run DDRv tool OK.

 

Case 2: using Nand boot, run serdes configuration project, when probe target -> read target fail as file attack below.

 

Case3: using Spi boot, run serdes configuration project. Results: the same case 2.

 

Software have license.

 

Please, support this issue, assa.

 

Brg,

Labels (1)
0 Kudos
Reply
1 Reply

1,470 Views
addiyi
NXP Employee
NXP Employee

Please provide a ccs verbose log when trying to read from target.

Adrian

0 Kudos
Reply