SerDes configuration issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SerDes configuration issue

1,626 次查看
tungnguyen
Contributor I

Dear Sir/Madam,

 

I have the problem on QorIQ for T2080 "serdes configuration when probe targget when using codewarrior tap". I try 3 cases:

 

Case 1: using Nand boot, run DDRv Tool. Results: probe target is ok, i run DDRv tool OK.

 

Case 2: using Nand boot, run serdes configuration project, when probe target -> read target fail as file attack below.

 

Case3: using Spi boot, run serdes configuration project. Results: the same case 2.

 

Software have license.

 

Please, support this issue, assa.

 

Brg,

标签 (1)
0 项奖励
回复
1 回复

1,532 次查看
addiyi
NXP Employee
NXP Employee

Please provide a ccs verbose log when trying to read from target.

Adrian

0 项奖励
回复