Sample Source code for MPC7410

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sample Source code for MPC7410

3,452 次查看
Muneer
Contributor II
hi

I'm using CW8.7 and my target is MPC7410
Any sample source code avaible as a project...
i tried in CW8.7 samples, in that i'm not getting any idea...

plz suggest me, where i can get sample...

Muneer
标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,830 次查看
J2MEJediMaster
Specialist I
It's not clear to me why you need a sample project targeting a specific processor. What CPU feature are you trying to make use of?

---Tom

0 项奖励
回复

1,830 次查看
Muneer
Contributor II
Hi

I'm new to this processor...
Actually i need boot code, basic register settings in MPC7410.
To MPC7410 processor Flash is interfaced for this how to do settings & what are all registers to be init

Muneer
0 项奖励
回复

1,830 次查看
Black
Contributor I
I recommend creating a stationery project with CodeWarrior EPPC New Project Wizard and Freescale PowerPC EABI Linker for MPC7410 and your evaluation board then add your own code to this project that can be used as a starting point. The stationery project has the minimal setup and code to get your evaluation board up and running. For more details please consult the stationery project readme files.
 
Please note that the current version of CodeWarrior for Power Architecture is 8.8.1 and it is available for download as an evaluation version here.
0 项奖励
回复