Program NAND flash CW 5.9.0 (windows) MPC8313ERDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program NAND flash CW 5.9.0 (windows) MPC8313ERDB

4,919件の閲覧回数
medina
Contributor III
Hello,
    I can program NAND flash from u-boot but cannot from CW. I switch SW3 and SW4 to use CW and CS0 to NOR. I follow this steps:

1- Select micro, USB TAP and init file (Freescale\CodeWarrior PA V8.8\PowerPC_EABI_Support\Initialization_Files\PQ2\8313RDB_init.cfg)
2- Select NAND flash (K9F5608U0D or K9F5608U0D_WITH_SPARE) and put base address (0xf8000000 from init file)
3- Erase and blank check.
4- Program binary file (u-boot-nand.bin) to NAND address base (0xf8000000).
5- Verify failed and when I try to boot it failed too.

Any advice or suggestion on what is wrong ? Any help will be welcome.

Thank's in advance.

Regards.

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,164件の閲覧回数
simon_ou
Contributor I
Hi, medina:
 
            I got it. Thanks a lot for your help.
 
 
 
            Simon ou
0 件の賞賛
返信

2,164件の閲覧回数
simon_ou
Contributor I
Hi, Tom & medina:
    
           I have met the same problem when i burn u-boot to the nand flash in the MPC8313ERDB board using CW 5.9.0.
 
           Could you tell me which package that need to patch the CW 5.9.0?
0 件の賞賛
返信

2,164件の閲覧回数
medina
Contributor III
Hi Simon,
    You must use the utility "CodeWarrior updater" from Start Menu. I don't know other way.

Medina
0 件の賞賛
返信

2,164件の閲覧回数
J2MEJediMaster
Specialist I
I've checked with an engineer here and the consesus is that you should file an SR on this. Click here to do that.

---Tom

0 件の賞賛
返信

2,164件の閲覧回数
medina
Contributor III
The Freescale support advised me to patch the CW. That was the solution. Now I can program NAND flash from CW.

Thanks Tom.
0 件の賞賛
返信