QorIQ T1024rdb debug error: cc not present

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ T1024rdb debug error: cc not present

1,749件の閲覧回数
cengizhanyapici
Contributor I

Hello

I  try to debug a bareboard project by using codewarrior tool.

My board is t1024rdb and I received it with linux installed. I have installed codewarrior tap to the board successfully. TX/RX led is solid RED. TX/RX led is green flashing.

I created a bareboard application with CodeWarrior wizard. Then I selected debug menu item. But, it returns an error: cc not present. I also noticed that whenever debug session is started, TX/RX led becomes solid redfor about 3 seconds and then it flashes green.

Best Regards

ラベル(1)
0 件の賞賛
返信
1 返信

1,542件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Cengizhan Yapicioglu,

Which OS do you use on you PC? Windows or Linux?

Do you use CodeWarrior TAP or the old product USB TAP?

CodeWarrior TAP integrates both USB and Ethernet ports, USB TAP only integrates USB port.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信