QorIQ T1024rdb debug error: cc not present

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ T1024rdb debug error: cc not present

1,750 Views
cengizhanyapici
Contributor I

Hello

I  try to debug a bareboard project by using codewarrior tool.

My board is t1024rdb and I received it with linux installed. I have installed codewarrior tap to the board successfully. TX/RX led is solid RED. TX/RX led is green flashing.

I created a bareboard application with CodeWarrior wizard. Then I selected debug menu item. But, it returns an error: cc not present. I also noticed that whenever debug session is started, TX/RX led becomes solid redfor about 3 seconds and then it flashes green.

Best Regards

Labels (1)
0 Kudos
Reply
1 Reply

1,543 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Cengizhan Yapicioglu,

Which OS do you use on you PC? Windows or Linux?

Do you use CodeWarrior TAP or the old product USB TAP?

CodeWarrior TAP integrates both USB and Ethernet ports, USB TAP only integrates USB port.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply