when I install QCVS in eclipse. this error has been occurred.
I use QCVS for qoriq power version 4.5.0.00001 . the eclipse version is "Eclipse IDE for C/C++ Developers 4.4.2".
Any body can help me.
An error occurred while collecting items to be installed
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.freescale.qcvs.feature_root 4.5.0.0001-20160210, action=).
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.
thanks.
已解决! 转到解答。
The correct update site for installing QCVS + FSL Updater is http://freescale.com/lgfiles/updates/Eclipse/QCVS for only ARM support or http://freescale.com/lgfiles/updates/Eclipse/QCVS_PA for QCVS 4.5 release including ARM + PA support.
Please refer to QCVS Installation Guide, chapter 3.2.
Adrian
I had a similar problem with the same error message ! Juno 4.2 + QCVS for qoriq power version 4.5.0.00001
So I follow advices fromaddiyi which are good, but I omited to install the "Eclipse Freescale Solutions Category" first. That was my second problem.
So,
Everything work fine .
Hi
I use eclipse 4.2 Juno.
I find "Eclipse Freescale Solutions Category" at Processor Expert Software, Microcontroller Driver S|NXP and install it.
and then I try to install QCVS but it error "No action found for: com.freescale.updater.customActions.freescaleprocesscheck."
I cant use from this link : http://freescale.com/lgfiles/updates/Eclipse/QCVS_PA .
I think that "Eclipse Freescale Solutions Category" has mistake. where can I download it?
The correct update site for installing QCVS + FSL Updater is http://freescale.com/lgfiles/updates/Eclipse/QCVS for only ARM support or http://freescale.com/lgfiles/updates/Eclipse/QCVS_PA for QCVS 4.5 release including ARM + PA support.
Please refer to QCVS Installation Guide, chapter 3.2.
Adrian