QCVS DDR configuration options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS DDR configuration options

Jump to solution
2,316 Views
PaulWalker
Contributor IV

Re: CodeWarrior 10.5 for Power Arch with QCVS

I'm using the DDR Configuration tool from QCVS to configure for DDR3L.

I'm trying to add config for extended temperature self-refresh (ASR/SRT). My MR2 value (SDRAM_MODE_2) is always zero. Where do I configure for self-refresh?

Also, how is DDR_SDRAM_INTERVAL calculated? My device datasheet (IS46TR16128DL) specifies a refresh interval of 8K cycles. How do I achieve this?

Thanks

0 Kudos
Reply
1 Solution
2,266 Views
yipingwang
NXP TechSupport
NXP TechSupport

In Properties panel in QCVS DDR tool, please click "Advanced" at the right top of the panel, then go to "SDRAM  Mode Configurations"->"SDRAM mode 2(MR2) - DDR SDRAM. Please refer to my screenshot as the following.

yipingwang_0-1695199310794.png

 

 

View solution in original post

0 Kudos
Reply
1 Reply
2,267 Views
yipingwang
NXP TechSupport
NXP TechSupport

In Properties panel in QCVS DDR tool, please click "Advanced" at the right top of the panel, then go to "SDRAM  Mode Configurations"->"SDRAM mode 2(MR2) - DDR SDRAM. Please refer to my screenshot as the following.

yipingwang_0-1695199310794.png

 

 

0 Kudos
Reply