Net Comm GA 4.4 Error for P1022

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Net Comm GA 4.4 Error for P1022

37,525件の閲覧回数
nishad_kamdar
Contributor IV

Hi,

 

I downloaded the GA 4.4 and installed it on my computer.

 

I am using Code Warrior PA 10.3.

 

When i follow the steps for importing the build project for P1022, and i Select the root directory,

 

It gives me an error saying that  "No Projects Found to Import" however for some other builds like 3041, once i select the root directory it gives me a list of the available

use cases.

 

What might be the problem? Does CW 10.4 not support P1022?

 

Moreover the P1022 build also does not seem to have the RCW folder which other builds have

 

Kindly advise..

ラベル(1)
3 返答(返信)

37,420件の閲覧回数
addiyi
NXP Employee
NXP Employee

QorIQ low-end cpu, as the one used in P1022, not used RCW file, so the RCW folder is not necessary for this processor.

Adrian

37,420件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Projects in bare_1022_cw_build have been saved as CodeWarrior Classic Projects format(for CodeWarrior 8.8), if you want to import these projects in CodeWarrior 10.3, please use use File->Import->CodeWarrior->CodeWarrior Classic Projects.

37,418件の閲覧回数
nishad_kamdar
Contributor IV


hello ,

Thank you for your time and support,

sorry for the late reply,

we had some other hardware issues with our board.

we have now got them solved.

Now we are trying to get the device drivers running for our custom p1022 board.

I followed the procedure which you have suggested. However, in the process of importing, in the access path window,

the code gives unresolved access paths for two Targets.

I have attached the snapshot of the same.

How can i resolve these access paths?

0 件の賞賛
返信