N25Q256 Flash Programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

N25Q256 Flash Programmer

ソリューションへジャンプ
2,888件の閲覧回数
jasonhendrix
Contributor V

We are building a custom board with an LS1020a processor and an attached N25Q256 QSPI flash.  The target tasks/flash programmer interface shows the N25Q128 (which I have used on the TWR dev board) and the N25Q512.  I found this document on how to add a flash chip to CW 10: Adding a new Flash Device to Codewarrior 10.x

 

When I navigate to the xml files described in that doc, I see that for algorithm, the N25Q128 uses N25Q128_QSPI.elf.  Can I use this .elf as well for the N25Q256?  I would provide a new xml file and modify the manifest as described in DOC_94792.

Interestingly, the N25Q512 xml file calls out N25Q512_QSPI.elf as it's algorithm, but no such file was installed in my CW installation.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,105件の閲覧回数
addiyi
NXP Employee
NXP Employee

N25Q128_QSPI.elf algorithm can be used with the mention that protect and unprotect action will not works correctly. But, erase/program/dump should works well.

You have to create a new XML, with the correct configuration for the new device.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,106件の閲覧回数
addiyi
NXP Employee
NXP Employee

N25Q128_QSPI.elf algorithm can be used with the mention that protect and unprotect action will not works correctly. But, erase/program/dump should works well.

You have to create a new XML, with the correct configuration for the new device.

Adrian

0 件の賞賛
返信