Medical USB compiling issues under CW V10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Medical USB compiling issues under CW V10

ソリューションへジャンプ
2,011件の閲覧回数
admin
Specialist II

Anyone successfully compile and run the Medical USB demo on a Flexis JM demonstration board (DEMOJM) using Code Warrior V10?

 

I am trying but I am getting too many errors that I don't understand.

 

Examples:

Description Resource Path Location Type
illegal implicit conversion from 'struct  *' to 'unsigned char *' khci.c Host_HID_example/User_Files/Source line 653 C/C++ Problem

 

Description Resource Path Location Type

illegal implicit conversion from 'struct  *' to 'unsigned char *' khci.c Host_HID_example/User_Files/Source line 653 C/C++ Problem

 

Description Resource Path Location Type

illegal implicit conversion from 'struct  *' to 'int *' khci.c Host_HID_example/User_Files/Source line 554 C/C++ Problem

 

I am also coming up with a bunch of warnings:

 

Description Resource Path Location Type

implicit arithmetic conversion from 'int' to 'unsigned long' khci.c Host_HID_example/User_Files/Source line 262 C/C++ Problem

 

Description Resource Path Location Type
implicit arithmetic conversion from 'long' to 'unsigned short' khci.c Host_HID_example/User_Files/Source line 354 C/C++ Problem

 

I am new to using CW tools and it's been a while since I was coding, so I may be making a novice mistake in the setup.  Any suggestions are welcomed.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,450件の閲覧回数
admin
Specialist II
0 件の賞賛
返信
1 返信
1,451件の閲覧回数
admin
Specialist II
0 件の賞賛
返信