LS2085Ardb: Downloading u-boot using Codewarrior cwtap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2085Ardb: Downloading u-boot using Codewarrior cwtap

1,942件の閲覧回数
ramasubramanian
Contributor II

Hi,

Do you have any guide describing the steps on how to download a custom built u-boot to LS2085Ardb using codewarrior cwtap?

Please point us to relevant application note for bringup of 2085A based custom board

 

Thanks

Rams

ラベル(1)
4 返答(返信)

1,665件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

Please use our last CodeWarrior for ARMv8 (2016.01 - 11.2.0) and make next steps:

1. open it using fsl_eclipse.bat from CW_ARMv8

2. make a new TCC configuration and use the Connect button

pastedImage_0.png

3. after connecting to the board, just use the Flash Programmer button

pastedImage_1.png

pastedImage_2.png

Thank you,

Marius

1,665件の閲覧回数
ramasubramanian
Contributor II

Hi,

I am using CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA Version: 11.1.1.  I am unable to get connect button in TCC configuration.  Do you recommend to install CodeWarrior for ARMv8 (2016.01 - 11.2.0)?

Thanks

Rams

0 件の賞賛
返信

1,665件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi Rams,

To be honest I recommend 11.2.0 (our last release) because it has also Flash Programmer GUI support.

If you want to continue with 11.1.1 please read in the Targeting Manual (from CW_ARMv8\ARMv8\Help\PDF) in chapter 7, how to use FP from gdb cmd line (don't scary, it's pretty easy are there are only 3 steps you need to do).

Best regards,

Marius

0 件の賞賛
返信

1,665件の閲覧回数
ramasubramanian
Contributor II

Hi Marius,

Thanks.  We now downloaded 11.2.0. We will test and let you know if we have any problems.

Regards

Rams

0 件の賞賛
返信