Kernel Aware Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Aware Debug

4,788件の閲覧回数
dferbas
Contributor I
Hi,

does anyone know if a sample kernel aware debug plugin exists ? I mean a package where I should implement only APIs described in Kernel-Aware_Debug_API.pdf and all other things (code skeleton with loading symbols from .elf, communication with target board over BDM) are already prepared ?

Thanks

Dusan
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,508件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Hi Dusan,

Well, where do you have the Kernel-AwarePluginManual.pdf from? I would check the same souce for samples as well.
To my knowledge the CodeWarrior COM Kernel Aware debugger API was only delivered to certain 3'rd parties and was never publicly available.

Daniel
0 件の賞賛
返信

2,507件の閲覧回数
dferbas
Contributor I
Hi,

this .pdf can be found among other manuals with every ColdFire CodeWarrior IDE. There is also .chm file. In the past I ported MetroTRK onto MC68EN302 for our OS. So I think I am expertized enough to do such a job. It's a pitty that such a plugin is not publicly available. Can we buy it ?

Dusan
0 件の賞賛
返信