How to use byte_swap.tcl script ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use byte_swap.tcl script ?

ソリューションへジャンプ
2,549件の閲覧回数
dhruvalkumarpat
Contributor III


I need to swap binary RCW file to load into QSPI flash . I tried to use byte_swap.tcl scrip and it gives me error . can you please let me know how to use  byte_swap.tcl effectively.

 

Thanks

Dhruval

ラベル(1)
1 解決策
2,171件の閲覧回数
dhruvalkumarpat
Contributor III

Thanks a lot . I thin when I run it as a script in linux I need to add following line at the top of script

#!/usr/bin/tclsh

Without this line It was giving me error . After I added this line It worked for me

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,172件の閲覧回数
dhruvalkumarpat
Contributor III

Thanks a lot . I thin when I run it as a script in linux I need to add following line at the top of script

#!/usr/bin/tclsh

Without this line It was giving me error . After I added this line It worked for me

0 件の賞賛
返信
2,171件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Dhruvalkumar Patel,

The script byte_swap.tcl is provided in Linux SDK, you could run "bitbake change-file-endianess-native", and get this script in the folder build_ls1043ardb/tmp/sysroots/x86_64-linux/usr/bin/byte_swap.tcl, I attached it for you.

Please use this script as the following

$tclsh  byte_swap.tcl  rcw_qspiboot.bin  rcw_qspiboot_swap.bin  8


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------