How to enter a "Custom" configuration value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enter a "Custom" configuration value

3,312 次查看
danmoffatt
Contributor II

What procedure is required in order to be able to enter a Custom configuration value in the CodeWarrior TAP tool PBL component as opposed to selecting one of the drop down menu items?

I have done it in an old LS1088A project but I forget the procedure/syntax to incorporate it in a new project that I am currently working on.

PBL Custom Value.PNG

0 项奖励
回复
7 回复数

3,283 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I installed CodeWarrior for ARMv8 11.5.12, and found there was no option for "0b10 Custom value".

In your IDE, you could select "skip error checking" to continue your configuration.

yipingwang_0-1675845975794.png

 

0 项奖励
回复

3,276 次查看
danmoffatt
Contributor II

Thank you for your reply.

Yes once the custom value is entered then you have to skip error checking in order to build the code.

The real issue is that the CodeWarrior tool has a fault in that it provides the RCW bits 212-211 binary setting as 0b01 for selecting the System Clock as the DDR_REFCLK_SEL.  The correct binary setting is 0b10 and hence a custom value needs to be entered in the tool settings.

danmoffatt_0-1675864755768.png

 

0 项奖励
回复

3,263 次查看
yipingwang
NXP TechSupport
NXP TechSupport

It seems that this is a defect of CodeWarrior for ARMv8 11.5.12, I have reported this defect to QCVS PBL tool development team.

0 项奖励
回复

3,307 次查看
KalaimaniArumugamdev
Contributor III

Hi @danmoffatt 

Refer "QCVS PBL Tool User Guide" chapter " 1.1.1.2.1 Specifying custom values".

 

Thank

Kalaimani Arumugam 

0 项奖励
回复

3,272 次查看
danmoffatt
Contributor II

Hi

Unfortunately, the "Ignore Constraints and non-critical Errors" option is not selectable for me (i.e., it is "greyed" out).

0 项奖励
回复

3,300 次查看
danmoffatt
Contributor II

I have downloaded the document and will give it a try.

Thank you very much!

0 项奖励
回复

3,298 次查看
KalaimaniArumugamdev
Contributor III
Great
0 项奖励
回复