How to debug target initialization file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to debug target initialization file

1,620 Views
zheng
Contributor II

My board use LS1043a and DDR3.  DDR4 is used on LS1043ARDB. How to modify and debug the "target initialization file" to fit my board? There are some print commands in the script file, but I don't know where the results are displayed.

0 Kudos
Reply
1 Reply

1,483 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello leon zheng,

Please modify the following section in CodeWarrior initialization file.  You could use QCVS DDRv tool to assist you to create a DDR project for your custom board and config DDR properties according to your target board, then use DDRv tool do validation to get the optimized parameters to use them to modify the following section.

def Init_DDRC():
    # SDRAM_CFG
    CCSR_BE_M(0x1080000 + 0x110, 0x450C000C)

    # CS0_BNDS
    CCSR_BE_M(0x1080000 + 0x000, 0x0000007f)
    # CS0_CONFIG
    CCSR_BE_M(0x1080000 + 0x080, 0x80010322)

    # TIMING_CFG_0
    CCSR_BE_M(0x1080000 + 0x104, 0xD0550018)
    # TIMING_CFG_1
    CCSR_BE_M(0x1080000 + 0x108, 0xC2C68C42)
    # TIMING_CFG_2
    CCSR_BE_M(0x1080000 + 0x10C, 0x0048C114)
    # TIMING_CFG_3
    CCSR_BE_M(0x1080000 + 0x100, 0x020C1000)
    # TIMING_CFG_4
    CCSR_BE_M(0x1080000 + 0x160, 0x00000002)
    # TIMING_CFG_5
    CCSR_BE_M(0x1080000 + 0x164, 0x04401400)
    # TIMING_CFG_7
    CCSR_BE_M(0x1080000 + 0x16C, 0x13300000)
    # TIMING_CFG_8
    CCSR_BE_M(0x1080000 + 0x250, 0x03115600)

    # SDRAM_CFG_2
    CCSR_BE_M(0x1080000 + 0x114, 0x00401010)

    # SDRAM_MODE
    CCSR_BE_M(0x1080000 + 0x118, 0x01010214)
    # SDRAM_MODE_2
    CCSR_BE_M(0x1080000 + 0x11C, 0x0)

    # SDRAM_INTERVAL
    CCSR_BE_M(0x1080000 + 0x124, 0x18600618)

    # DDR_WRLVL_CNTL
    CCSR_BE_M(0x1080000 + 0x174, 0x8655F606)

    # DDR_WRLVL_CNTL_2
    CCSR_BE_M(0x1080000 + 0x190, 0x05070600)
    # DDR_WRLVL_CNTL_3
    CCSR_BE_M(0x1080000 + 0x194, 0x0)

    # DDR_CDR1
    CCSR_BE_M(0x1080000 + 0xB28, 0x80040000)
    # DDR_CDR2
    CCSR_BE_M(0x1080000 + 0xB2C, 0x0000A181)

    # SDRAM_CLK_CNTL
    CCSR_BE_M(0x1080000 + 0x130, 0x02000000)
    # DDR_ZQ_CNTL
    CCSR_BE_M(0x1080000 + 0x170, 0x8A090705)

    # SDRAM_MODE_9
    CCSR_BE_M(0x1080000 + 0x220, 0x00000400)
    # SDRAM_MODE_10
    CCSR_BE_M(0x1080000 + 0x224, 0x04000000)

    # CS0_CONFIG_2
    CCSR_BE_M(0x1080000 + 0x0C0, 0)

    # SDRAM_CFG
    CCSR_BE_M(0x1080000 + 0x110, 0xC50C000C)

Thanks,

Yiping

0 Kudos
Reply