How do I disable T1042 serdes plls in Codewarrior?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I disable T1042 serdes plls in Codewarrior?

1,239 Views
robwestfall
Contributor II

How do I disable the T1042 Serdes PLLs in Codewarrior?


We do not have any hardware that uses the Serdes on our custom board and need to disable it as the board is stuck in a reset loop if this isn't set.  We can set it with the USB Tap, but that obviously isn't product intent.

 

The T104x manual says in Section 31.1.1.3 Disabling Unused SerDes Modules:

SerDes is disabled as follows:

• SRDS_PLL_PD_S1 = 11 (both PLLs configured as powered down)

• SRDS_PLL_REF_CLK_SEL_S1 = 00

• SRDS_PRTCL_S1 = 0xFF

(no other values are permitted when both PLLs are powered down)

 

How do I do this in the RCW so that it happens on CPU reset?  The CodeWarrior QCVS has GUI selections for these fields, but I can't specify 0xFF for the SRDS_PRTCL_S1 Field, I can only select from the GUI options.

 

Thanks,

Rob Westfall

Labels (1)
0 Kudos
Reply
1 Reply

1,063 Views
addiyi
NXP Employee
NXP Employee

To be able to use any custom values for RCW fields in PBL tool you should select the Advanced tab, then Ignore Constrains and non-Critical Errors.

pastedImage_0.png

In this way, when you will select the SRDS_PRTCL_S1 field, you'll see the Custom Bitfiled Value option.

pastedImage_1.png

Enter the value, select the Custom Bitfiled Value and Apply.

Adrian

0 Kudos
Reply