HLP: Problem in C++ throw().....

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HLP: Problem in C++ throw().....

1,557 次查看
tkvenki
Contributor III

Hi All,

 

I'm using Codewarrior for Coldfire - Version 6.4 Build 6.

I have created a sample C++ project, which does a try-throw catch.

But when the control reaches throw() the program will terminate(will exit from debugging session completely!!!).

 

The Controller I'm using is MCF5485

 

Please find the following files attached:

1. InstalledPlugins.txt - For Platform related information

2. main.c - The sample source code.

 

Please help me out....

 

Thanks and Regards,

Venkatesh

 

Installed Plugins.TXT

main.c

Message Edited by t.dowe on 2009-09-04 02:59 PM
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

759 次查看
tkvenki
Contributor III

I tried out this code in a standard C++ compiler...It works...

Are there any  settings I have missed in CW ??

 

0 项奖励
回复

759 次查看
tkvenki
Contributor III

I have raised a service request on 22-JUN

But I did not get any response till now......

 

Let me know, if I can help in re-creating the error...

 

 

 

0 项奖励
回复