GCC toolchain for P2020

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GCC toolchain for P2020

ソリューションへジャンプ
3,896件の閲覧回数
ericfornstedt
Contributor III

Hi,

 

We have a project using the P2020 processor where we need to switch to a GCC toolchain instead of the Freescale PPC toolchain, for example gcc-4.9.2-Ee500v2-eabispe. For a number of processors you can choose to use either Freescale PPC or GCC toolchain when creating a new project in CodeWarrior (10.5.1), but for the P2020 the GCC toolchain is not available for some reason.

 

So, how can we switch to a GCC toolchain for the P2020? There are many source code files (and linker file) in a P2020 project template that have Freescale PPC compiler specific syntax and therefore cannot be compiled with GCC right away. Are there templates suitable for P2020 and for GCC elsewhere we can use?

 

BR

/ Eric

タグ(4)
0 件の賞賛
返信
1 解決策
3,887件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please create a bareboard project for P2020DS, then modify Toolchain configuration from Project->Properties->C/C++ Build->Toolchain Editor.

Please configure Current toolchain as: PowerPC EABI e500v2 C Toolchain Release.

Current builder as: PowerPC EABI e500v2 Release Builder

There is no template for P2020 GCC toolchain, you could create a bareboard project for P4080DS to do reference.

元の投稿で解決策を見る

タグ(1)
2 返答(返信)
3,858件の閲覧回数
ericfornstedt
Contributor III

Thank you,

Using the information from a P4080DS build we were able to do the necessary changes for our P2020 build.

0 件の賞賛
返信
3,888件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please create a bareboard project for P2020DS, then modify Toolchain configuration from Project->Properties->C/C++ Build->Toolchain Editor.

Please configure Current toolchain as: PowerPC EABI e500v2 C Toolchain Release.

Current builder as: PowerPC EABI e500v2 Release Builder

There is no template for P2020 GCC toolchain, you could create a bareboard project for P4080DS to do reference.

タグ(1)