Scan timeout during secure debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Scan timeout during secure debug

2,303件の閲覧回数
SergioS
Contributor II

Dear all

I've configured a LS1012A board to manage secure debug (level 2)

When I try to connect to target CCS and CodeWarrior studio return the error "Scan timeout"

I've seen that this bug is documented in the release notes of 11.2 version (DTCCS-124

Issue: [LS1043][SecureDebug] CCS returns Scan timeout when trying to
config chain

Workaround: none

Now I'm using v11.5.5 but the problem is the same. Does anybody know the status of this bug?

Thanks and regards

Sergio

0 件の賞賛
返信
1 返信

2,271件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信