Flash Programmer problem, Codewarrier MobileGT V9.2, MPC5121

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programmer problem, Codewarrier MobileGT V9.2, MPC5121

Jump to solution
1,787 Views
martinw
Contributor III

Hi,

 

We currently have 2 Codewarrier installations, both MobileGT V9.2 and on identical PC's running XP pro.

 

The flash programmer on my installation doesn't give me an option for the 5121.

 

In the tools/flash_programmer window the only option in the Processor Family box is grayed out and contains "ALL". The target processor box contains "AXE" with no other options.

 

Also the second time I try to run Flash Programmer I get the following error message:
 
"flash programmer plugin failed to initialize, a default configuration file ffdeviceconfig.xml containing the supported device list was not found, or was found with invlaid content.  Please contact Freescale support."
 
I have totally removed CodeWarrier from my machine and re-installed it, but nothing changed.  


The other CodeWarrier installation doesn't have AXE as an option, but offers processor family 5200 with 5121 as an option in the target processor box.

 

I raised a service request, and was told to try the demo software from the web.  I haven't done that yet as it's the same version as mine (9.2).

 

Any idea what could have gone wrong with my installation?

 

Regards

Labels (1)
0 Kudos
Reply
1 Solution
1,037 Views
martinw
Contributor III
sorted - I had to browse to the correct configuration file (.xml) under the codewarrier installation.

View solution in original post

0 Kudos
Reply
1 Reply
1,038 Views
martinw
Contributor III
sorted - I had to browse to the correct configuration file (.xml) under the codewarrier installation.
0 Kudos
Reply