Codewarrier MobileGT V9.2, connection to debugger problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrier MobileGT V9.2, connection to debugger problem

1,829 次查看
martinw
Contributor III

Hello,

 

When connecting to my target using USB TAP, if the target power is missing then CodeWarrier reports a problem but seems to 'hang' after that.

 

I have to Ctrl-Alt-Delete to kill CodeWarrier.

 

Regards

 

Martin Wakely

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,129 次查看
ronco
NXP Employee
NXP Employee

Hi Martin,

 

So, what, that's a problem?   :smileytongue:

 

Try this: look for the dark-grey "CodeWarrior Connection Server" icon in your Windows Tooltray.  This icon appears whenever the debugger is started.  When you get a lockup, try right-clicking the CCS icon to close it.  Kill it if you have to.  This may save your CodeWarrior IDE.

 

You're right, though, this shouldn't be happening.  I think we need a Service Request to formally address the issue.  When you create it, please add two things:

 

  - In your USB TAP configuration panel there's an "Enable logging" feature.  Turn that on, start the debugger, capture the Log window's contents and send that in.

 

  - In the CodeWarrior IDE select Help->About->Installed Products->Save As and include the resulting text file.

 

I hope this helps.

 

-Ron

0 项奖励
回复

1,129 次查看
martinw
Contributor III

Hi Ron,

 

I'll try that, and I'll also post a service request with the log.

 

Regards

0 项奖励
回复