Evaluation Codewarrior DDR validation and internal RAM flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Evaluation Codewarrior DDR validation and internal RAM flash

2,084件の閲覧回数
winstonjacob
Contributor IV

   I am using Codewarrior evaluation version and the codewarrior tap device, and I am not able to do the DDR validation, Nor flash  and internal RAM flash are not working on LS1021a processor, so can anybody conform, whether I need to buy a licensed version or not.

 

Regards

Winston

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,080件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The evaluation license provides full features of CodeWarrior and DDRv tool, however the evaluation license will expire after 15 days.

You need to purchase license for CodeWarrior and DDRv tool from https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

 

0 件の賞賛
返信

2,054件の閲覧回数
winstonjacob
Contributor IV

When I run DDR validation test in evaluation board, we are getting response as result as 0%  all the time.

can you share the procedure to do the DDR validation in ls1021atwr board?

 

Regards

Winston.

0 件の賞賛
返信