Evaluation Codewarrior DDR validation and internal RAM flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Evaluation Codewarrior DDR validation and internal RAM flash

2,153 次查看
winstonjacob
Contributor IV

   I am using Codewarrior evaluation version and the codewarrior tap device, and I am not able to do the DDR validation, Nor flash  and internal RAM flash are not working on LS1021a processor, so can anybody conform, whether I need to buy a licensed version or not.

 

Regards

Winston

标记 (3)
0 项奖励
回复
2 回复数

2,149 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The evaluation license provides full features of CodeWarrior and DDRv tool, however the evaluation license will expire after 15 days.

You need to purchase license for CodeWarrior and DDRv tool from https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

 

0 项奖励
回复

2,123 次查看
winstonjacob
Contributor IV

When I run DDR validation test in evaluation board, we are getting response as result as 0%  all the time.

can you share the procedure to do the DDR validation in ls1021atwr board?

 

Regards

Winston.

0 项奖励
回复