ERROR: Invalid/unsupported hardware problem  !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR: Invalid/unsupported hardware problem  !

Jump to solution
1,447 Views
kvl
Contributor I

thx

Labels (1)
0 Kudos
Reply
1 Solution
1,323 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Murali Kondapi,

Do you use CodeWarrior for PA 10.5?

Which processor do you use?

Do you use CodeWarrior JTAG configuration file to override RCW function? If so, please note that the processor type in the JTAG file is the same with the project and your target.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,324 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Murali Kondapi,

Do you use CodeWarrior for PA 10.5?

Which processor do you use?

Do you use CodeWarrior JTAG configuration file to override RCW function? If so, please note that the processor type in the JTAG file is the same with the project and your target.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply