ERROR: Invalid/unsupported hardware problem  !

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ERROR: Invalid/unsupported hardware problem  !

跳至解决方案
1,448 次查看
kvl
Contributor I

thx

标签 (1)
0 项奖励
回复
1 解答
1,324 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Murali Kondapi,

Do you use CodeWarrior for PA 10.5?

Which processor do you use?

Do you use CodeWarrior JTAG configuration file to override RCW function? If so, please note that the processor type in the JTAG file is the same with the project and your target.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,325 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Murali Kondapi,

Do you use CodeWarrior for PA 10.5?

Which processor do you use?

Do you use CodeWarrior JTAG configuration file to override RCW function? If so, please note that the processor type in the JTAG file is the same with the project and your target.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复