ERROR: Invalid/unsupported hardware problem  !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR: Invalid/unsupported hardware problem  !

ソリューションへジャンプ
1,461件の閲覧回数
kvl
Contributor I
ラベル(1)
0 件の賞賛
返信
1 解決策
1,337件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Murali Kondapi,

Do you use CodeWarrior for PA 10.5?

Which processor do you use?

Do you use CodeWarrior JTAG configuration file to override RCW function? If so, please note that the processor type in the JTAG file is the same with the project and your target.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,338件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Murali Kondapi,

Do you use CodeWarrior for PA 10.5?

Which processor do you use?

Do you use CodeWarrior JTAG configuration file to override RCW function? If so, please note that the processor type in the JTAG file is the same with the project and your target.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信