DQ Mapping must be indentical between two DDR controllers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DQ Mapping must be indentical between two DDR controllers?

ソリューションへジャンプ
3,609件の閲覧回数
Simon666
Contributor II

our ddr memory is 16GB with ECC, every one ddr controller connect 8GB, dram chip is MT40A1G16.

but our DQ Mapping is different between two ddr controllers, when I config dq mapping will get error like this:

 

Simon666_0-1660719537647.png

 

0 件の賞賛
返信
1 解決策
3,590件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The LX2 HW /registers for each controller is independent of each other and setting different DQ mapping for each controller is possible. but the existing released SW allows for only one (the same) DQ mapping for both controllers.

元の投稿で解決策を見る

1 返信
3,591件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The LX2 HW /registers for each controller is independent of each other and setting different DQ mapping for each controller is possible. but the existing released SW allows for only one (the same) DQ mapping for both controllers.