Connecting to target board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting to target board

ソリューションへジャンプ
4,427件の閲覧回数
Irfan3
Contributor III

Hello team,

I am using code warrior v10.5 for my t2080rdb board for debugging. Can you help me in connecting the board to the code warrior through software. I have connected the probe and tap by the help of codewarrior tap user guide but unable to connect the hardware through ide for debugging. Do you have steps for connecting and then debugging uboot. 

 

 

 

 

0 件の賞賛
返信
1 解決策
4,397件の閲覧回数
Irfan3
Contributor III

Hi Yipingwang,

Thanks for your quick response.

I had followed the code warrior probe tap user guide for setting the probe with the host and the target. My assumption is that you have taken it as hardware connections.

My question is related to the target hardware+code warrior kit and code warrior IDE connection. How will i come to know whether my target is connected to the IDE. Are there any steps for setting up the connections and i am using code warrior over USB as connection type and not Ethernet.

Please feel free to ask if you didn't understand my question

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,387件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

As I mentioned previously, first please create a bareboard "hello world" project, then check whether you could connect this project to the target board.

Please refer to sections "3.2.1 Creating CodeWarrior Bareboard Application Project" and "3.4.1 Debugging Bareboard Application Projects" in C:\Freescale\CW_PA_v10.5.1\PA\Power Architecture Processors Getting Started Guide.pdf to create and debug a bareboard project

タグ(1)
0 件の賞賛
返信
4,379件の閲覧回数
Irfan3
Contributor III

Hi Yipingwang,

Sorry for missing that. After installing code warrior the first step was to execute the inbuild example "Hello world"  and we were able to see the output on tera term(Terminal).

Thanks to your information i was able to connect to the target and see the information on the IDE.

Last one question, after adding breakpoint and if i click on "resume to line" in diassembly the information present in disassembly vanishes and it doesn't stop. can you provide help on these.

 

0 件の賞賛
返信
4,411件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to sections "3.2.1 Creating CodeWarrior Bareboard Application Project" and "3.4.1 Debugging Bareboard Application Projects" in C:\Freescale\CW_PA_v10.5.1\PA\Power Architecture Processors Getting Started Guide.pdf to create and debug a bareboard project.

For u-boot debugging, please refer to the section "7.6 Debugging U-Boot using NOR, NAND, SPI, and SD Card/MMC Flash Devices" in C:\Freescale\CW_PA_v10.5.1\PA\Help\PDF\Targeting_PA_Processors.pdf.

You could refer to "debug u-boot for e500mc" sections in this step by step application note https://community.nxp.com/t5/CodeWarrior-Development-Tools/CodeWarrior-U-Boot-Debugging/ta-p/1121398...

0 件の賞賛
返信
4,398件の閲覧回数
Irfan3
Contributor III

Hi Yipingwang,

Thanks for your quick response.

I had followed the code warrior probe tap user guide for setting the probe with the host and the target. My assumption is that you have taken it as hardware connections.

My question is related to the target hardware+code warrior kit and code warrior IDE connection. How will i come to know whether my target is connected to the IDE. Are there any steps for setting up the connections and i am using code warrior over USB as connection type and not Ethernet.

Please feel free to ask if you didn't understand my question

0 件の賞賛
返信