Codwarrior crashes when attempting connect to 5208EVB via USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codwarrior crashes when attempting connect to 5208EVB via USB

2,895 Views
wermgerl
Contributor I
I have a eval 5208 eval board and a usb multilink from P&E but can't seem to get them to connect
When I select "connect" from the debug menu, I get a message that says "Select port number within valid range"  And then codewarrior crashes with an  unhandled exception.
 
I've set the target up to use the factory defaults for PEMICRO_USB.
 
 
I've downloaded installed the latest drivers from P&E
Any hints on what to try next? 
Labels (1)
0 Kudos
Reply
1 Reply

1,239 Views
marc_paquette
Contributor V
What version of CodeWarrior for ColdFire do you use?
 
Marc.
0 Kudos
Reply